Other Parts Discussed in Thread: SN65LVCP114
Hello,
In order to extend the amount of switch options of my transceiver interfaces I would like to place two SN65LVCP114 back-to-back. The channel between the two switches will be very short < 1 inch. If I understand correctly there is a risk of over-equalizing. Is it recommended to add some ISI? Besides increasing the length of the channel, are there other feasible, and controlable options to do this?
Thanks,
Ingmar van Klink