Other Parts Discussed in Thread: TUSB3410
Dear Roberto,
I have a problem with the TUSB3410 too, but different. The funny part is that I had a problem on my former system (XP 32-Bit) too, but somehow I solved it with the help of Dr. Google - around 3 years ago. This time I can't find any solution. My system is Win 7 x64 Ultimate SP1 (all Updates as by today).
I am using an USB-2-Serial cable (came with a Huawei Terminal Adapter for CDMA) which gets identified as TUSB3410 Device (COM7). The driver is 6.7.2.0 from 03/20/2013...no problems during installing...
Now I want to use the cable (as I did before on XP as well) as a bridge between a MCU Device I build and Putty...
If I hook the MCU direct to the build in RS232-Port (COM1) on my PC - it works...if I use the TUSB3410 cable with the same setting (COM7) no data gets transmitted. I even tried all different setting (XON/XOFF etc. FIFO ON/OFF, Change of COM-Port to COM2...etc,etc,etc...) There is no data transfer...even I used another similar cable (I have around 40 of them here) - no transfer....
Unfortunately I sampled some of the TUSB3410 Chips last month and was about to integrate them in my MCU application...but if the customers later will face this kind of problems to connect/access - I have to reconsider....
I hope you can help me to find a solution, coz I don't want to mix within my MCU App...almost all components are TI...
Thx...
Dr. Klaus Helmgens