Is it necessary to solder GNDPAD to PCB for normal IC operation?
Or is GNDPAD intented only for extension of temperature range?
Thanks.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi Alexander,
Yes, it is necessary to solder the GNDPAD to the PCB for proper operation.
Regards,
Ross
TI offers DP83848C which doesn't have this pad. So I assume -YB version has it for thermal dissipation purposes only. Am I right?
Does GNDPAD have any connection to analog or digital ground inside the chip?
DP83848YB datasheet states that I should solder this pad if I want to get +125 °C temperature range. But what if temperature will never rise above +70 °C? Would DP83848YB with unsoldered GNDPAD be equivalent to DP83848C?
Thanks.
Hi Alexander,
You are correct that the GNDPAD is just for thermal purposes. We recommend that the user solder the pad for maximum performance. I am not sure why you would use the YB unless you wanted temp range above 85C. If you are worried about soldering the GNDPAD but want similar specs to the YB, our DP83848I is another alternative.
Regards,
Ross