Other Parts Discussed in Thread: DS92LV0411, DS90C383, DS92LV0412, DS90CF384, LV24EVK01, DS92LV0421
I previously make a design using the DS92LV0411/412 IC to serialize 4 Ch+1Clk LVDS so that I can transmit it over fiber optic cable. My initial design was as follows. The LVDS data is 24 bpp video with a resolution of 640x480.
Source (DS90C383) -> DS92LV0411 -> Maxim MAX3840 2x2 CML Crosspoint Switch -> Finisar FTLF1319F1HTL SFF Module -> Single Mode fiber optic cable -> Finisar FTLF1319F1HTL -> Maxim MAX3840 2x2 CML Crosspoint Switch -> DS92LV0412 -> Destination (DS90CF384)
I had an issue where the video would flash on and off when only a black background with some text was on screen, but when the video switched over to a camera feed the video was non existent on the screen. Taking advice from a previous post and redesigned the board directly connecting the DS92LV0411 and 412 (with coupling capacitors) to trouble shoot, but I had the same issue as previously stated.
I decided to try a few eval boards to make sure a flaw in the PCB's I had made was the source of the problem.
When using the LV04EVK01 kit, the video is steady with the text and black background, but no video presents on the screen when the source is a camera stream. The source and destination are still the same but withe the eval kit in between.
I also tried using the LV24EVK01 kit in conjunction with the CLINK3V28BT-85 eval kit. This setup looks as such:
Source (DS90C383) -> CLINK LVDS Rx'er Board -> LV04EVK01 CML Tx'er Board -> LV04EVK01 CML Tx'er Board -> CLINK LVDS Tx'er Board -> Destination (DS90CF384)
I get the same results as the first and second setup. Flashes of the video stream with black background and red text, and nothing with a camera feed.
In all cases when the camera feed is on the LVDS stream the LOCk led is not steady. It flashes very rapidly. I am unsure why I am losing the lock on the clock signal.