Other Parts Discussed in Thread: SN65HVD230
Hi,
I have a question about CAN Tranceiver SN65HVD230.
In datasheet page.8 "RECEIVER ELECTRICAL CHARACTERISTICS",
there are Rdiff(Differential input resistance) and RI(CANH, CANL input resistance).
Each resistance value is as following:
Rdiff : 40kΩ to 100kΩ
RI : 20kΩ to 50kΩ
Is these resistor integrated inside the SN65HVD230(internal resistor) or
should the user need to install on the board?
best regards,
g.f.