Other Parts Discussed in Thread: LMH0046, LMH0002, LMH0302
We are looking for SMPTE serialize specification:
a) IC has to support the out format SMPTE 259 M class A 480i
b) the output is comming to a BNC connector
c) Cable type is coaxiial cable with impedance of 75 ohms
d) single channel output.
So we have shortlisted the part code(LMH0046), the challenge I could fore see is the output on 75 ohm coaxial cable.
Kindly confirm if the same part code can comply to requirement ,else suggest the par code which can meet the requirement.