This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

[ DS90UB928 ] Delay from RIN to Valid Back Channel Communication



[ DS90UB928 ] Delay from RIN to Valid Back Channel Communication

Hi,

Do you have any numbers which describe the delay in between valid RIN  and achieving valid back channel communication? Please see drawing below. Is it same delay that until having valid data output (tDDLT)?

Also, is there any ways to calculate this Lock Time more accurately as per PCLK frequency? My customer would like to enable the back channel communication as soon as link is recovered. 

Other reference and related discussion.
[ DS90UB928 ] Delay from RIN to TxCLKOUT/TxOUT
http://e2e.ti.com/support/interface/high_speed_interface/f/138/p/354834/1244675.aspx#1244675
 
Thanks,
Ken
  • Hi,

    I hope you enjoyed holiday last week.

    It's greatly appreciated, if you can look into the discussion above.

    Feel free to contact with me, if necessary.

    Thanks,
    Ken
  • Hi Ken,

    The I2C back channel communication will be available as soon as lock is established. So when Lock pin goes high, you can start sending back channel I2C commands.

    The lock time is related to the PCLK frequency, but we don't disclose the internal workings of the locking mechanism. It will be longer at lower PCLK frequencies and shorter at higher PCLK frequencies.

    Thanks,
    Jason