Other Parts Discussed in Thread: DS100BR410
Hello,
What is the exact internal pull-up pull-down resistor value for the DS100BR410 pins
1. BST_2 internal pull-up
2. BST_1 internal pull-up
3. BST_0 internal pull-down
4. EN_3..0 internal pull-up
5. PIN_MODE internal pull-up
6. OOB_DIS internal pull-down
7. Are direct connections to VDD and GND recommended - or do you recommend a 1k pull-up/pull-down for the above and all other select pins (CS, DE_SEL, VOD_EL etc..aside from the 20k that is already recommended in datasheet)?
8. IF the following pins SD3..0, CS, SDC, SDA are No Connects, do you see any issues?
Thanks for your help.
- Lopa