Other Parts Discussed in Thread: TCA9617A, TCA9509, TCA9517
Hi,
The application that is intended to develop makes use of two sensors connected individually using FFC cable to the base board. There is another sensor, which is placed on the base board itself. The length of the FFC cable (or the distance between the base board and the two sensors) is 70mm. These three sensors has to be configured using I2C. But the driving strength of the processor is less to drive 3 devices.
Which I2C buffer operating at 3.3v will drive three devices, out of which two are placed at a distance of 70mm?
Thanks