Other Parts Discussed in Thread: TUSB9261
Hello,
Now, I connect in SATA. But I investigate that I connect via USB3.0-SATA bridge LSI.
I have two questions about TUSB9261.
1.
Please teach me the following specifications. (I hope for a result using exerciser to exclude performance of SATA device oneself.)
Throughput: the result of CrystalDiskMark
Latency: the result of bus analyzer of USB and SATA.
2.
Please tell me whether performance deteriorates in comparison with a case of the SATA connection when I publish what kind of command. (Please tell the deterioration degree if possible.)
Regards,
Daisuke