Other Parts Discussed in Thread: DS90UB914A-CXEVM
We are using the DS90UB914A-CXEVM evaluation board. We want to configure the deserializer registers through I2C but we don't get to access to these registers. The I2C address of the deserializer by default in the evaluation board is supposed to be 0x60 and we are using the I2C peripheral master of a Zynq platform in the Zedboard evaluation board. We connect the SDA, SCL, VREF (3.3 V) and GND from the Zedboard to the DS90UB914A-CXEVM I2C interface.
We don't know if it is something wrong in the configuration: the signal levels? the connection to the board? the I2C address? the I2C signals? something in the board configuration?
Any suggesstion?
Thank you very much in advance.