Other Parts Discussed in Thread: LMH0341, LMH1983, LMH1981, THS8200
Hello;
I am looking for a way to detect the start of video frame in any of the standard SDI video inputs. The signal will be used as the synchronized trigger for another camera. The latency between the actual video frame and the trigger should be less than 0.7 ms.
I also noticed that THS8133 is obsolete. I am thinking of using LMH0341, but unsure whether this is the best IC or no. I am wondering is there any simpler method to detect the start of frame than de-serializing the input. I will be thankful if you can inform me about any alternative IC or Method.
Thanks,
Nikoo