Other Parts Discussed in Thread: TUSB9261
We are having a problem when we use drives larger than 2 TB with the TUSB9261.
When we format a drive using either GPT or MBR mode using the TUSB9261 and then take that same drive and connect it's SATA port directly to the system without the TUSB9261 the volume the was created does not show up in Windows. Is there any limitation of drive capacity when using the TUSB9261? Has it been tested with drives larger than 2 TB?