This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PCIe GbE switch connection



I am searching for a integrated solution to connect a gigabit ethernet
switch via PCIe:

* Host: PCIe x1
* Switch: RGMII

As far as I understand, a network interface controller without PHY is
what I need. Do you have anything in your product range that can be used
in my case?

The component selection regarding the switch is also to be determined.
These are the features required:

* >= 6 copper GbE ports
* 1 (R)GMII port to be connected to the host using PCIe
* VLAN tagging