Other Parts Discussed in Thread: SN6501, TPS55010
Hello,
I need an isolated DCDC converter to provide 3V3 @ up to 5mA. The idle load will be only around 100uA, and the primary side power budget is an average load of just 250uA. So Quiescent supply and minimum load are important factors.
Is the SN6501 a suitable choice? It has a typical no load current of 150uA, but it's hard to tell from the data sheet what the total supply current would be for a load of 100uA as the efficiency curve (page 1) tends to 0% as the load approaches 0.
Another option may be the TPS55010, which has a higher quiescent supply of 360uA. This figure is sufficiently low that together with the convenient enable and soft start features would make power cycling a viable option as a typical duty cycle would be around 10% active.
Are there better chips for my application? Perhaps for such a low maximum load, capacitive or optical solutions might be adequate?
Thanks, Ross