Other Parts Discussed in Thread: TUSB2077A, TPS2041
Hello,
I have a newly developed board with a TUSB2077A and a TPS2041 on it.
I had connected the Enable input of the TPS2041 to pin 36 (PWRON7) of the TUSB2077A but the downstream-power would not be switched on.
After connecting the Enable input to pin 23 (PWRON4) of the TUSB2077A everything works fine.
I measured the voltages of the PWRON-pins of the TUSB2077A and saw that the PWRON-pins 1 to 4 are low and pins 5 to 7 are high.
Which PWRON-pin shoudl I use when the USB-hub is configured in ganged-mode. I would expect all PWRON-pin behave the same.
Thank you already for your answers.
Regards,
Wamor