Other Parts Discussed in Thread: DS100DF410, DS100BR410
Hi,
the manual for DS100DF410 retimer claims that it is pin-compatible with DS100BR410 redriver. I am trying to design my board so it would initially be used with DS100BR410, but can support DS100DF410 if necessary. It is not entirely obvious how certain pins have to be connected to provide such compatibility.
Specific questions:
| pin # | pin in BR410 | pin in DF410 | connection details and questions |
| 24 | GND | LPF_REF_2 |
connected to capacitor 22 nF per DF410 manual. However, this means that BR410 will have that GND pin not connected to GND. Is this OK? |
| 13 | VDD | LPF_REF_3 |
connected to capacitor 22 nF per DF410 manual. However, this means that BR410 will have that VDD pin not connected to VDD. Is this OK? |
| 39 | SD3 | GND |
left unconnected. Cannot connect to GND because in BR410 this is an output. This means that DF410 will have this pin not connected to GND. Is this OK? |
Thanks.