Other Parts Discussed in Thread: TFP410
so the datasheet for this part isn't clear on some stuff for me and i'm still wet behind the ears with this part so bear with me.
the DE generator is a little confusing as to what it really does.
i understand it handles the data enable state for the system so if there is no DE signal going into this thing you can still write to the panel. if i am wrong on that please correct me.
one thing that it looks like it might also do is handle positioning the image on a bigger screen so your oddball image (say 1024x600) can sit in the middle of a 1280x720 screen. is that right? is that the point of the DE_TOP and DE_DLY? it would make sense based on my interpretation of the graphic on page 16 of the datasheet. the main screen is in the middle surrounded by a black border that is DE_DLY and DE_TOP many pixels big...right? if i am wrong then what is the true purpose of DLY and TOP?
also my question on the V_RES and H_RES values. one thought i had was that they represent the pixel height and width of the image you are trying to output, right? but they are not the pixel dimensions of the image i am actually putting out there so it makes me think these numbers represent the biggest i can get using this configuration? are one these ideas right? if they represent the biggest i can output then are the values adjustable if i change clock frequencies?