This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

XILINX VIRTEX5 SERDES - TLK2711



I have a XilinxV5 Eval board with the on chip SERDES interface. I am building a TLK2711 board which will interact with the V5 SERDES links. I can see that V5 is a CML logic ,while 2711 is a VML device. So if I use an AC coupling on the board that I am building, will that be sufficient ?