Other Parts Discussed in Thread: DP83848C
Dear Sir,
We are using DP83848C ethernet PHY communicating with LPC2478.
We are connected PHY in RMII mode.
I got following results on different pins.
- PFBOUT (pin 23) connected to PFBIN1+2 (pins 18, 37) and having 1.8V
- PWR_DOWN (pin 7) is High
- MDC (pin 31) No clock
- MDIO (pin 30) shows 3.3V
- 25MHZ_OUT (pin 25) has 50 MHz (correct, because in RMII mode)
- RX_DV/RMII_MODE (pin 39) is pulled up to VCC(3.3V) by 2.2k, signal is permanetly low (plausible cause no packets received)
- RBIAS (pin 24): 1.2V
- 0V on PHYAD0 - PHYAD4