Other Parts Discussed in Thread: SN65HVD232, TS3DS10224, SN74CBT3306C, SN74CBT3306, TS5A9411
Hello,
As per my project requirement, i need to disconnect and connect the CAN bus with one control signal. My customer needs CAN bus open failure condition to be simulated. I am planning to use Analog/digital Switch between CAN Bus and CAN Transceiver, so that i can open the switch when failure has to be simulated.
i have browsed TI products, but couldn't find switch specifically for CAN BUS. Since there are many switches available, i am totally confused in which one to select. I am using SN65HVD232 CAN transceiver, data rates upto 1 Mbps, two 120 Ohms at both the ends of CAN Bus.
Kindly suggest suitable switch. I need your suggestion.
Thanks in advance.
Regards,
Govind.