Other Parts Discussed in Thread: TLK1221
For the TLK1221 ETHERNET TRANSCEIVER, what is the LVTTL output impedance for the RD[9:0], RBC[1:0] and SYNC/PASS outputs?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: TLK1221
For the TLK1221 ETHERNET TRANSCEIVER, what is the LVTTL output impedance for the RD[9:0], RBC[1:0] and SYNC/PASS outputs?
Hi Lee,
Output impedande value is not specified in datasheet but it should be in the 30 - 50 Ohm range. Even datasheet mentions:
"The primary application of these devices is to provide building blocks for point-to-point" baseband data transmission over controlled-impedance media of 50 Ohms"
Regards!
Luis Omar Morán Serna
High Speed Interface Group
SWAT Team