This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DS90UB925 repeate rmode cancel



Hi, My customer want to use the device as “74MHz clock with 18-bit RGB mode”. So the MODE_SEL pin should be ; LFMODE=L, I2S Cannel mod B=H, This setup is #3 configuration only in the Table 4. About the #3 config., the device must be a repeater mode, but customer wants to use the device as Display mode as below, CPU --- ‘925 -----‘928 ---- LCD Is it possible to use the device as a Display mode under #3 configuration? Or please let me know which config is fit for “74MHz clock with 18-bit RGB mode” ?