Other Parts Discussed in Thread: SN65MLVD205A
I have a design based on the AD part and I am trying to replace it with the SM65MLVD205AD.
One issue that has been raised during a peer review was the ESD ratings. The AD part states 15kV HBM and 8kV Contact (absolute maximum). The TI part only states "Bus Pin ESD Protection Exceeds 8 kV". Is it HBM?
The second question related to the first one is what I should do to guarantee the replacement (if done) does not compromise the robustness of the design.