Other Parts Discussed in Thread: TUSB9261
Dear support-team,
I noticed that there's a new default firmware version 1.05 for TUSB9261 available. Currently, we are using version 1.04 in our embedded device (TUSB9261 is connected via USB3.0 hub to a SigmaDesigns SX6). Now I like to know what have changed from v1.04 to v1.05 to decide whether to update or not. I have downloaded and 'installed' the firmware package already, but unfortunately there's no change log included.
Background: We have complains about the TUSB9261 sometimes not being recognized by the SX6 while the hub is there. However, these cases are very seldom and at the moment I can't say which part is responsible: SX6 host, hub chip (SMSC 5534b) or the TUSB9261. But maybe the firmware update can help?
Thanks and best regards, Christian.