This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

SN75DP130 - Unused pins

Guru 19785 points

Other Parts Discussed in Thread: SN75DP130

Hi Team,

Could you please let me confirm how to treat the following unused input/output pins of the SN75DP130DS ? I am thinking that these pins could be left open.

Pin 8 : CAD_SRC
Pin 9 : HPD_SRC
Pin 33 : SCL_DDC
Pin 34 : SDA_DDC

Best Regards,
Kawai

  • Hello Kawai,

    Indeed, it is possible to leave the DDC pins unconnected when you use the SN75DP130 in DP-only mode. For the CAD_SRC pin, you can either leave it unconnected or controlled by CAD_SNK (depending on the implemented ode and the GPU options). HPD_SRC can also be unconnected, however the customer must take into account how tho handle the hot plug detection.

    It would be useful if you share the specific case, then I can provide a precise recommendation for the customer.

    Best regards,
    Diego.