Other Parts Discussed in Thread: DP83640
Hi,
I'm looking at the DP83640 device and it looks really appealing in terms of IEEE1588 performance. The only issue though is that I'm looking specifically for a 24.576MHz clock output (for audio applications) from the device but this is not available as a divisor of the 250MHz.
Does anyone know of a way to get a synchronized 24.576MHz clock from the device? One thing, for example, I was looking at was setting the output frequency to 10MHz and using a GPS to audio clock converter to do the rest - but I'd rather do it in one go if at all possible.
Best Regards,
Ken