This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Device with ISO5500 driver modification



Hi,


I made a MOSFET driver with ISO5500 and I used two voltage sources: -15V and +15V. Now I want to modification my device and use only +15V.

I attach schema. On the blue colour is the first schema, and modification is on the red. Can I short point 18 and 19 and drop out - 15V source only? Have I drop out C6 and C3?  Will it work?

Thank You very much for help.