This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

RS-485 Transceiver with IEC61000-4-2/IEC61000-4-4 protection

Guru 29720 points
Other Parts Discussed in Thread: SN65HVD1470, SN65HVD70

Hi Team,

My customer is looking for the RS-485 transceiver.
The requirement of the device is the following.
-------------------------
- supply volatge: 5V
- No. of TX/Rx: 2/2(ideal) or 1/1
- Duplex: full
- IEC61000-4-2 Contact Discharge: 8kV
- IEC61000-4-4 Fast Transient Burst: 1kV
-------------------------
Is there any TI device that meets this requirement?
I couldn't find the device on TI web...

Best Regards,
Yaita / Japan disty