Hello,
I came across SN65LVPE502 EVM, which also has a board schematics.
1. I will be using SN65LVPE512 in my application. Can I use the 502 board schematic as a reference to my design?
There is something I`m not so sure about at the 502`s board schematics, it seems that the polarity of the Tx and Rx pairs is inversed twice. For example:
USB3_TX_P (pin at the connector side) ---> RX1_N (pin at the 502 device)
TX1_N (pin at the 502 device) ----> USB3_RX_P (pin at the connector side)
Same thing about the other pair.
My question is, why is it in reverse polarity?
When using the SN65LVPE512, do I need to inverse the polarity as well?
Will my application work correctly if I will not inverse the polarity?
Thanks and regards,
Gil