Other Parts Discussed in Thread: DP83640, TMS320C6454
Hi,
I have a hardware with DP83640 PHY and following are the details:
- The DP83640 PHY is interfaced to LAN9215i (MAC) through MII mode.
- The LAN9215i has parallel interface to DSP (TMS320C6454).
- The LAN9215i configuration is completed. The device ID and other MAC registers configured properly.
- But, PHY configuration is not happening. I'm not able to read or write to any of the PHY registers. Also, the 100Mbps link gets established, 25MHz clock MII_TX and MII_RX clock outputs are available.
Kindly, let me know if there is any specific hardware strapping that needs to be taken care.