Other Parts Discussed in Thread: TLK110
Hi,
I have problem with TLK110 PHY to make it operate properly. I have designed a hw board which uses almost the same configuration as the f28m36 controlCard. For the RJ45 connector I use the Pulse JXR1-0011NL, which has very similar parameters to J0011D01BNL which is used on the controlCard. The communication between the PHY and the MCU is working properly and I can also read the auto-negotiation information of the remote device, but for some reason in the PHYSTS (0x0010) register I read cleared bits at 10, 9, 0. -> Signal is not detected, Descrambler Lock is not indicated and Link is not established. All these bits are set in the case of controlBoard.
Do you have any idea what can be the problem, or any suggestion how can I find it out.
Thanks in advance!
Best Regards,
Tamas