This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TCA6424A - confusion about address



Ok, I have this GPIO expander hung off my MSP430s I2C bus, and I read the data sheet but I'm puzzled.

It says that the address is 0 1 0 0 0 1 ADDR R/W (Section 8.3.3).. then immediately after in Table 3 it says the address is either 0x22 or 0x23.

Uhm, 0 1 0 0 in the high nybble is 0x40.  Unless this is HIGH to LOW and not LOW to HIGH, which is REALLY confusing.

Can anyone shed some light on this?

Ed Averill