Other Parts Discussed in Thread: TMDS442
I am designing in the TMDS442 for a customer of mine. Two inputs will be used and both outputs which will both select the same input.
When in I²C control mode and Source Plug-In Status Register Bit Decoder Bit 4 (5V_EN) is set to 1. Does this then override the OE for the sink port - Bit 2 in the Sink Port Register Bit Decoder and enable the TMDS output selected by Bits 0-1 when a Hot Plug is detected in the Source Plug-In Status Register (Bits 0-3)?
When in I²C control mode, unless I have missed something, there does not seem to be a register bit to detect Sink Hot Plugging. In port control mode, the status is available on pins 49 and 68. I was trying to design in power save features in that the appropriate sink OE would only be active when hot plugged. In the design, one HDMI sink will be active all the time and the other on demand.