Other Parts Discussed in Thread: TUSB2046B, TPS2044, TUSB2036
We are planning to use TUSB2046B in our project and have some issue need to be clarified.
1. In our application , our USB device are all self-power mode. We don't need TPS2044 power chip.
How should we do about PWRONx# and OVRCURx# pins ??
PWRONx# maybe can be folating , because PWRONx# in output.
How about OVRCURx# ?? pull-high or others ?
2. What function is external EEPROM used for ? IS only for recordind custom ID and vender ID ?
Need to use external EEPROM to save config setting when TUSB2046B power-on ?
3. In our case , all USB device are self-power mode. BUSPWR need to pull low right ?
How about EEDATA/GANGED pin set ?
4. We only use two port. Please help to give us some suggestion about two port USB-Hub chip datasheet.
Thanks!!