Other Parts Discussed in Thread: DS125DF1610
Hi,
I wish to have non CDR data output.
I set channel registers
0x09 = 0x20
0x1e = 0x01
However, no data is output unless the CDR is locked.
Thanks,
Greg
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS125DF1610
Hi,
I wish to have non CDR data output.
I set channel registers
0x09 = 0x20
0x1e = 0x01
However, no data is output unless the CDR is locked.
Thanks,
Greg
Hi Mike,
Thanks for your reply. I set the pre, main, and post cursors as you suggested above. Here is a register dump that shows signal detect and CDR lock. Data is output.
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: 00 80 dc 00 01 01 01 01 60 20 50 6f 08 b4 93 69
10: 3a 20 e0 90 00 13 7a 36 40 20 a0 03 90 00 00 55
20: 00 00 00 40 00 01 bd 37 b4 60 30 0f f2 01 00 f6
30: 00 58 11 88 bf 1f 30 00 10 00 00 3e 33 00 2c 80
40: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90
50: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5
60: 33 be 00 00 00 00 00 a0 00 0a 22 40 00 00 00 00
70: 03 00 10 10 10 10 22 1a 30 10 00 00 00 48 13 3a
80: 3f e4 00 00 a4 00 00 00 00 00 26 00 00 02 1c 00
90: 00 00 00 00 00 00 3c 00 0c 3f 3f 00 d5 99 96 a5
a0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90
b0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5
c0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90
d0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5
e0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90
f0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 02 00 03 01
Here is a register dump that shows signal detect and no CDR lock. Data is not output.
0 1 2 3 4 5 6 7 8 9 a b c d e f
00: 00 80 84 00 01 01 01 01 60 20 50 6f 08 b4 93 69
10: 3a 20 e0 90 00 13 7a 36 40 20 a0 03 90 00 00 55
20: 00 00 00 40 40 01 6e 00 00 00 30 0f f2 01 00 f6
30: 00 58 11 88 3f 1f 30 00 00 00 00 00 00 00 2c 80
40: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90
50: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5
60: 33 be 00 00 00 00 00 a0 00 0a 22 40 00 00 00 00
70: 03 20 00 00 00 00 22 1a 20 10 00 00 00 48 13 3a
80: 00 e4 00 00 a4 00 00 00 00 00 26 00 00 02 1c 00
90: 00 00 00 00 00 00 3c 00 0c 3f 3f 00 d5 99 96 a5
a0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90
b0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5
c0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90
d0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 d5 99 96 a5
e0: 00 01 04 10 40 08 02 80 03 0c 30 41 50 c0 60 90
f0: 88 82 a0 46 52 8c b0 c8 57 5d 69 75 02 00 03 01
Thanks for our help,
Greg
Hi Greg,
Since the data rate you would like to operate at is not supported by this device there will be a limitation on the features that you can use. The CDR is required to create clocks for the DFE, FIR and CTLE adaption. If the CDR is not able to lock then these features become unavailable. This means that you will need to operate with manual CTLE configuration and no FIR and DFE.
For application requirements I would use the following sequence:
| Register | Write Value | Write Mask | Comment |
| 0xFF | 0x00 | 0xFF | Select share registers |
| 0x02 | 0x-- | 0x60 | program desired ref clock input frequency |
| 0xFF | 0x01 | 0xFF | select desired channel register set |
| 0xFC | 0x-- | 0xFF | |
| 0xFD | 0x-- | 0xFF | |
| 0x00 | 0x04 | 0x04 | reset channel registers, this is self clearing |
| 0x0A | 0x0C | 0x0C | put CDR into reset |
| 0x14 | 0x40 | 0x40 | Force signal detect low |
| 0x1E | 0x00 | 0xE0 | configure the pfd mux to output raw data |
| 0x09 | 0x20 | 0x20 | enable override for pfd setting to take effect |
| 0x3D | 0x00 | 0x3F | zero out main cursor |
| 0x3E | 0x3F | 0x7F | maximize pre cursor and set polarity to true (non-invert) |
| 0x3F | 0x00 | 0x3F | zero out post cursor |
| 0x0D | 0x10 | 0x30 | Configure for 700mVpp VOD, set to either 5'h0F or 5'h0E. Bit 4 and 3 go to 0x0D[5:4], bit 2, 1 and 0 go to 0x2D[2:0] |
| 0x2D | 0x07 or 0x06 | 0x07 | |
| 0x31 | 0x00 | 0x60 | configure for adapt mode 0 |
| 0x03 | 0x-- | 0xFF | set desired CTLE value |
| 0x3A | 0x-- | 0xFF | |
| 0x0A | 0x00 | 0x0C | release CDR from reset |
| 0x14 | 0x00 | 0x40 | release signal detect force condition |
Some of the items above are precautionary commands and can possibly be removed. Please let me know if you have questions about this sequence.
Mike Wolfe
DPS Apps / SVA
Hi Garrett,
With regard to your question: If the CDR can’t lock (1.92GHz signal is not supported by the CDR module) can we operate the DFE, CDR, FIR in a bypass mode, so that 1.92GHz data can still be routed?
The sequence that Mike Wolfe provided you should allow you to do just what you are requesting. Per the sequence, the PFD mux is being configured for raw data mode (i.e. CDR bypass) and you are zeroing the post and main FIR taps while maximing the pre-cursor (this is the bypass routing scheme for the part.) Moreover you are setting the device to adapt mode 0 and manually entering EQ values. I did notice that the EQ override operation is not included in Mike's sequence. I would add that operation after your write operations to 0x03 and 0x3A.
By the way, what are the values that you are programming to registers 0x03 and 0x3A? Perhaps your values need to be adjusted to ensure proper operation. For 1.92GHz there should not be a high amount of EQ boost needed, particularly if the PCB channel is not that long.
Let me know if you have further questions.
Cordialy,
Rodrigo Natal
DPS Applications Engineer
Hi Mitch. I checked this function in the lab using a DS125DF1610 EVM board. When I provide 1.92GHz clock signal as input to DF1610 DUT channel, I can see its Tx output that data after configuring the device to raw mode while still operating in the default ref mode 3. The device does report that CDR is not locked on status register but the raw data output is present.
Regards,
Rodrigo Natal
DPS applications engineer
Hi,
The datapath flow for the DF1610 device is the following:
EQ -> XPOINT -> DFE -> CDR -> FIR -> Driver
Given the flow above, if you are multicasting channel 1 to channels 1 and 2 then you would need to set both channels 1 and 2 to PFD mux raw mode and adjust FIR tap values accordingly (i.e. zero main and post, max out the pre.) But once you do that, you should be able to see the data output on both channels for the default ref mode 3. I've double checked this on the bench with my DF1610EVM to confirm that I'm able to do it while passing 1.92GHz 1010 signal.
Regards,
Rodrigo Natal
DPS Applications Engineer
Hi Greg,
For my setup I set:
Cordially,
Rodrigo Natal
DPS Applications Engineer
Hi Greg, Garrett,
Were you able to resolve this issue?
Mike Wolfe
DPS APPS / SVA
Hi Rodrigo,
Thanks for your help.
Does this work if channel 5A is configured to operate as a slave (0x96 set to 0x3c). If not, why? When would slave mode be used?
Thanks,
Greg
Hi Greg,
You should always configure channel register 0x96 bit 5 to be master. Actual master control is assigned by mux selection. Slave mode is indeed intended for the scenario where the device is configured to have one-to-many connections and the channel in question is outputting data input to another channel. However, based on our functional verification we recommend always setting register 0x96 bit 5 for master (i.e. value of '0'.)
Rodrigo Natal
DPS Applications Engineer