This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

DP83865 100Mbps RGMII

Hi,

 I was wondering if this phy supports 100Mbps RGMII. There is no timing diagram for this mode on page 77 of the data sheet and Table 42 does not indicate that it's a valid controller i/f for 100Base-TX. The confusing part is that in section 6.5.1 in note 4 under the table, it says

"For 10 Mbps and 100 Mbps, Tcyc will scale to 400 +- 40ns and 40ns +-4ns". This would lead me to believe that 100Mbps RGMII is supported.

Thanks for clearing that up,

Amish