Other Parts Discussed in Thread: XIO2001
I'm designing miniPCIe module with XIO2001 and it is basically works well.
By the way, I have a question regarding power source of XIO2001.
According to "miniPCIe Electrical Specification", the host may supply the +3.3V in suspend/sleep mode but +1.5V may be turned off.
I've designed using +3.3V and +1.5V of host supply. Thus in suspend/sleep mode, the XIO2001's core voltage is turned OFF.
XIO2001's datasheet show power sequence only turn ON/OFF all of +3.3V and 1.5V at the same time.
Is this situation safe for XIO2001 or should I change the supply circuit so that generate +1.5V from +3.3V ? I've connected VDD_33_AUX to +3.3V also.