Other Parts Discussed in Thread: SN65LVCP114
Please help answer the following questions on the SN65LVCP114
1. By default on 10G SFI line, do I have to enable squelched or not? “ “FST_SW” line to high?
2. For controlling this device between using GPIO “Selx” lines or through I2C mode, which signals do I use to toggle between control by GPIO or by I2C?
3, Control by GPIO “SelX” do I need to use CS?
For I2C, do I need to set CS=”1” and Ic2_sel = “1”?
4. What are the minimum control lines do I need to set to switch between GPIO config or through I2C?
Thank you