This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TFP410

Guru 13485 points


Would like to work with voltage of 1.8V at the RGB inputs. According to the d/s if   the Vref voltage is  between   0.5V to  0.95V, I can work a minimum voltage of  Vref + 0.2, which means you can work at a voltage of 1.8V at the inputs.Please that I understood correctly.