Other Parts Discussed in Thread: MAX3221E
I have a simple low-speed multi-drop application where I have about a dozen nodes that need to listen and will only talk when spoken to by the master controller.
Is there an interface chip like the MAX3322E that is specifically for this application or can one of the many TI chips do this via the shutdown or enable pin?
I supposed I could put a diode on the transmit pin but then the speed and length of the cable would be very limited.