Other Parts Discussed in Thread: DP83816, DP83848-EP
Need infromation on DP83816 which is MAC+PHY device and IEEE 802.3 compliant. If designed/Used on the Board what all the tests need to be performed to meet the IEEE testing compliance when used on the board. need to get information on the test that needs to be done on teh board/pcb level so that the board will the IEEE testing conformance.