Other Parts Discussed in Thread: ONET1101L, ONET4201LD
Hi,
I am currently in need of a laser driver to power a laser diode. This is for an optical time of flight system where the laser beam is traveling through the air. This is only needed for output to the laser. The laser diode itself needs little input to power it (3V input, current rating of 40 mA), so practically any driver should work. I just need a driver that comes with an affordable evaluation module for testing purposes. Is there anything in your catalogue that fits this criteria?
Thanks,
Nathanael