Other Parts Discussed in Thread: DS90CF388A
Hi Team,
Do we have the LVDS receiver solution that can support 1080p and operating temperature from -40 to 85 degree C.
The DS90CF388A operating temperature is from -10 to 70 degree C.
Thanks,
Prescott
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: DS90CF388A
Hi Team,
Do we have the LVDS receiver solution that can support 1080p and operating temperature from -40 to 85 degree C.
The DS90CF388A operating temperature is from -10 to 70 degree C.
Thanks,
Prescott
Hi Prescott,
In order to operate at 1080p, you need data that is clocked at approximately: 1920 x 1080 x 60 (fps) x 1.2 (blanking interval) = 149.3 MHz, single pixel. If there is 28 bits per clock period being serialized, this equates to a throughput of 149.3 x 28 = 4.1804 Gb/s.
Unfortunately, none of the LVDS receiver solutions we have in the -40 to 85 C operating range can go up to this data rate. The only SerDes pairs we have that support this rate, whether in single pixel or dual pixel operation, are only consumer grade, so the temperature range of operation will not exceed -10 to 70 C.
Thanks,
Michael