This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Question about DP83865 twsted pair impedance

Genius 4250 points

Hi,

I'd like ask about DP83865(Giga Ether Phy) as follows,

In DP83865 D/S page66 5.7 Twisted Pair Interface,
There is some description about the twisted pair impedance as follows,

"50-Ohm controlled impedance with respect to VDD or GND"

While in the SNLA056D App note"DP83865 Gig PHYTER V 10/100/1000 Ethernet Physical Layer Design Guide"
page10 8 Twisted Pair Interface,

There is some description about the twisted pair impedance as well,
but the expression is silghtly different from that of in DP83865 D/S page66.

"50-Ohm controlled impedance with respect to AVDD"

which one is correct?

Thanks

Go

  • The Media Dependent Interface (MDI), also referred to as the Twisted Pair Interface (TPI), is biased from a 2.5V analog voltage supply.  This supply may be referred to as the Analog VDD (AVDD).  It is acceptable for the MDI traces to have a 50 Ohm characteristic impedance relative to either this 2.5V analog supply or to ground.  The most common approach is to reference ground.

    Patrick