This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLK110 Pin Strapping of LED pins



Hi,

The three outputs LED_LINK, LED_SPEED and LED_ACT also act as pin strapping for Auto-Negotiation. Strapping this pins as "1" is easy as the figure 3-6 in the actual datasheet shows. How about strapping this pins as "0"? Do the LED's automatically change polarity when strapping with Pull-Down resistor? If not, what is the right way to do that? Any example schematic for that?

Thanks and best regards,
Patrick