Other Parts Discussed in Thread: ISO1540
My customer wants to know if this configuration will work - see attachment.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: ISO1540
My customer wants to know if this configuration will work - see attachment.
Ignacio,
We're looking into this and will get back to you shortly.
Ignacio,
I don't see any issue with the configuration you have shown.Only point to take care is the that total capacitance on 12 inch cannot be more than 40pF. If this is more then the maximum speed of operation will be proportionally lower.
Regards,
Sarangan Valavan
Sarangan,
In relation to this question, what are the concerns in using the configuration below with two ISO1540 devices, where side 2 of both isolation devices is connected to the cable? Since side 2 can drive 400 pf, this configuration should be able to work bidirectionally, correct? Would there be any issues with side 2 of one device driving side 2 of the other device?
Hi James,
I don't see any issues with this configuration. Side2 of ISO1540 is completely I2C compliant. Side 2 of one device can drive Side 2 of another.
Rgds,
Anant