Other Parts Discussed in Thread: ALP
Hi,
1) Did the DS90UB913A / 914A need to be configure for the register setting using the SPA Dongle Board & ALP GUI every-time power on?
2) What's the purpose of the SPA Dongle & ALP GUI used for?
3) I've the TI eval board for 913A / 914A and connected to Aptina Camera module. Did the Ser & Der able to transfer camera data without any ALP GUI setting in the 1st time? Currently I don't have the SPA Dongle Board.
4) Current board are set to Pixel Clock input to Ser. Can I2C able to transfer bi-direction from Der to Ser in order Aptina DevWare to communicate or detect Camera module and then control the camera module setting on the fly?
5) At what setting and condition, data from Camera module able to transfer data from Ser -> Der and I2C able transfer bi-direction?
Thanks.