Other Parts Discussed in Thread: SN65LVDS100, SN75DP130
I want to connect the SN75DP130's AUN_SNK pins to the FPGA via the SN65LVDS100 voltage translator because the FPGA I/O banks only accepts 1.2V or 1.8V. Does anyone have recommendations on termination/coupling between the SN65LVDS100 and the SN75DP130? Also as a sanity check, does the connection from the DP130 to the FPGA seem reasonable using this translator?