Other Parts Discussed in Thread: ISO1050, ISO3082
Hi,
For long (600m) bus length CAN application, I am considering the ISO1050 CAN transceiver:
1- We need to support 10K to 125Kbps
2- We will need to support up to 70 devices on a bus.
Would like to know if there is a limit on the minimum bit-rate that the transceiver can handle?
What is the limit on number of devices (ISO1050) on the bus?
Thank,
Ran